Author Topic: Compilation Error 448  (Read 10325 times)

Offline mattz

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Compilation Error 448
« on: August 06, 2025, 05:19:23 PM »
I am somewhat new to Plus+1.  I received a project file, that I am trying to make a change too.  So I did not create a project/program from scratch.  I have taken the Fundamentals and Advanced trainings, but it was several years ago.  I made a small change to the program and I want to test it on a real world device.  I have made the change and (attempted to) compile the program.  Under the "Error/Warning/Hint Messages" the compiler says "COMPLETE - No specific issues identified".  However, the compiler message is giving me the error seen below, and I am not getting a downloadable plus1 file in my project folder to load into the ECU.  Has anyone seen this?  I am not ruling out an IT related measure that is preventing this from completing, since I have run into that already too.  Any help would be appreciated.

Offline llang

  • PLUS+1 Developer
  • ***
  • Posts: 10
  • Karma: +1/-0
Re: Compilation Error 448
« Reply #1 on: August 27, 2025, 02:06:54 PM »
I would try to create a new +1 project and copy the code from your file to the project. Then you can try to compile.

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 339
  • Karma: +29/-3
Re: Compilation Error 448
« Reply #2 on: August 28, 2025, 07:27:22 AM »
Hello mattz,

I have seen something like this when you exceed the memory of the unit you are using.
Remove a chunk of code and see if the compilation works. You can see how much memory you use in the compile message after a successful compilation.
!!  Please do a backup before doing this.   !!

If it doesn't work, please contact PLUS+1 Helpdesk. https://www.danfoss.com/en/campaigns/dps/plusplus1-support-form/

Have a nice day
Best regards,
Tor
PLUS+1® SW PAE Team