Author Topic: Compilation Error 448  (Read 10367 times)

Offline mattz

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Compilation Error 448
« on: August 06, 2025, 05:17:12 PM »
I am somewhat new to Plus+1.  I received a project file, that I am trying to make a change too.  So I did not create a project/program from scratch.  I have taken the Fundamentals and Advanced trainings, but it was several years ago.  I made a small change to the program and I want to test it on a real world device.  I have made the change and (attempted to) compile the program.  Under the "Error/Warning/Hint Messages" the compiler says "COMPLETE - No specific issues identified".  However, the compiler message is giving me the error seen below, and I am not getting a downloadable plus1 file in my project folder to load into the ECU.  Has anyone seen this?  I am not ruling out an IT related measure that is preventing this from completing, since I have run into that already too.  Any help would be appreciated.


Offline QWERTY

  • PLUS+1 Novice
  • *
  • Posts: 4
  • Karma: +0/-0
Re: Compilation Error 448
« Reply #1 on: August 06, 2025, 10:03:24 PM »
I've had the same issue before, and I closed and reopen the Plus 1 Guide and it went away. Sometimes I have to restart my computer for the error to go away.