Author Topic: Joystick model number 10103708 function block  (Read 11544 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 136
  • Karma: +2/-1
Joystick model number 10103708 function block
« on: May 14, 2025, 06:51:15 PM »
Hello Guys,

I want to use Joystic Danfoss model number #: 10103708.

What is it and where Can I find its function block or example in Plus+1 to use it.

Thanks in advance for your help

With best regards


Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 210
  • Karma: +38/-3
Re: Joystick model number 10103708 function block
« Reply #1 on: May 15, 2025, 08:34:16 AM »
I think it is a JS1000, but can't find any reference to the specific part number to tell if it is CAN or analogue.
https://www.danfoss.com/en/products/dps/electronic-controls/joysticks-and-foot-pedals/joysticks/js1000-light-duty-joystick/#tab-overview

The blocks can be downloaded via the Plus+1 Update Center. They are under Compliance Blocks | Joysticks

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 136
  • Karma: +2/-1
Re: Joystick model number 10103708 function block
« Reply #2 on: May 15, 2025, 06:22:32 PM »
Hello sir,

Thank you very much for your replay and information.

Yes it's from familly SJ1000.

With best regards

Offline G30RG3

  • PLUS+1 Expert
  • ****
  • Posts: 93
  • Karma: +4/-2
Re: Joystick model number 10103708 function block
« Reply #3 on: May 16, 2025, 05:45:07 PM »
Modelcode JS1000-XY-A-J331-BLSW
So a J1939 joystick with a node id 0x33, not redundant. 
Hardware/HMI/CANJoysticks/JS1000 CAN 10105531v104...