Author Topic: Compiling program changes without compiling images  (Read 23988 times)

Offline dudleyr

  • PLUS+1 Novice
  • *
  • Posts: 1
  • Karma: +0/-0
Compiling program changes without compiling images
« on: October 22, 2017, 05:17:03 PM »
Hello,

I'm wondering if there is a way to compile changes to my display program (for DP710) without compiling all the images being used. I try using the "Compile Changed" option, but almost every time the compilation goes through all the images as well even if I've only added a simple checkpoint to the program. As a result, compiling this display program takes about 7 minutes, with half of that being the images. This makes system debugging very tedious and time-consuming.

Thanks in advance for any suggestions.

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 210
  • Karma: +38/-3
Re: Compiling program changes without compiling images
« Reply #1 on: October 23, 2017, 09:05:20 AM »
I just tested this on my system with a program for the DP720 that takes about 2 minutes to compile. I added a checkpoint and complied using Compile Changed. This resulted in a compile time of under 30 seconds and none of the images were compiled.

I am using Guide version 9.1.7 and the DP720 hardware file is 70096706v200.

Alastair