Author Topic: CS10 - M2M - hide Functions?  (Read 1229 times)

Offline Nikkin

  • PLUS+1 Novice
  • *
  • Posts: 1
  • Karma: +0/-0
  • Almost a Plus+1 expert
CS10 - M2M - hide Functions?
« on: July 22, 2026, 09:25:24 PM »
Hello everyone!

I need your help configuring CS10.

I'm trying to connect four CS10"Station" units to a CS10 "access point" and receive messages at CAN0 port. Likewise, I need messages present on the CAN0 bus to be retransmitted to the Station modules. I have managed to do this, but only with two modules. Although the M2M protocol specifies a connection of only two, I would like to know if anyone has managed to do this and how.

I would be very grateful for any help.

Thanks a lot
Nikkin :)

Offline Lukey

  • PLUS+1 Guru
  • *****
  • Posts: 108
  • Karma: +12/-1
Re: CS10 - M2M - hide Functions?
« Reply #1 on: July 23, 2026, 02:36:43 AM »
The hardware cannot work like you described, as you mentioned only two device can connect to each other,, it's doesn't work like a broadcasting  master and slave/s.