Author Topic: USB Storage Device not recognized when using CG150-2 and Service Tool ?  (Read 23487 times)

Offline Lukey

  • PLUS+1 Guru
  • *****
  • Posts: 107
  • Karma: +12/-1
USB Storage Device not recognized when using CG150-2 and Service Tool ?

Hardware is DM1x00 Displays, I have tried on both a DM1200T and DM1000T with no success.

Has anyone encountered this?

I am NOT able read/write/see my USB Storage Device connected to the M12, C4—USB Host port when using a CG150-2 and Service Tool

I am able read/write/see my USB Storage Device when using the USB Interlink and Service Tool which is connected on the M12, C3—USB Device port

Offline SJones

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Re: USB Storage Device not recognized when using CG150-2 and Service Tool ?
« Reply #1 on: November 13, 2025, 12:02:54 AM »
I am having a similar issue with USB storage device,  did you ever find a solution?

Offline Lukey

  • PLUS+1 Guru
  • *****
  • Posts: 107
  • Karma: +12/-1
Re: USB Storage Device not recognized when using CG150-2 and Service Tool ?
« Reply #2 on: November 13, 2025, 04:13:32 AM »
I didn't not find a solution, i expect it's a hardware limitation, maybe the USB/Serial and CAN port are using some of the same hardware and don't allow the use of both devices concurrently ?

Helpdesk didn't not help me with this issue, i just worked around it.