Author Topic: Update center version  (Read 11397 times)

Offline federico.furlani

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Update center version
« on: January 26, 2026, 04:10:46 PM »
Hi,
why there was available the 1.0.190 version and now I can find only the 1.0.188?
Is there any problem?

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 340
  • Karma: +29/-3
Re: Update center version
« Reply #1 on: January 27, 2026, 07:49:40 AM »
Hello federico.furlani,

I'm guessing you mean that the download link for PLUS+1 Update Center contains version 1.0.188 and not 1.0.190?   Good question and I have no good answer for you.

This shouldn't really matter, because PLUS+1 Update Center should automatically update to the newest release after installation.

If you do update to 1.0.190, don't click the button in the web browser that shows up, I believe it confirms that you are logged in and the button should direct you to the PLUS+1 Tool. Just close the browser and use the tools you need.  Some user have got an error pop-up they need to confirm, but it ends up behind the Update Center Window and they can't click OK.  If this happens, use the task manager to end the tool and restart. It should work after that.
This issue is fixed in the next release.

Have a nice day.

Best regards,
Tor
PLUS+1® SW PAE Team

Offline federico.furlani

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: Update center version
« Reply #2 on: January 27, 2026, 01:35:19 PM »
Hi,
It matter for us because the installation is handled by our ICT dept and we need to put the installation of update center on our centralized system.
Can you fix it please?

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 340
  • Karma: +29/-3
Re: Update center version
« Reply #3 on: January 28, 2026, 07:17:41 AM »
Hello,

I have notified the responsible team and I hope it will be fixed in the near future.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team