Author Topic: Is there a method to use namespace in set value signal names?  (Read 9924 times)

Offline davidNeedsHelp

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +2/-0
Is there a method to use namespace in set value signal names?
« on: September 12, 2025, 05:43:14 PM »
Hey Community,


I've got a bunch of "linked" pages (linked in the sense that behaviour is the same, but they're not actually linked pages because of the reason here), with the only difference between being the namespace, and the fact that I have to manually go into each page to change the set value signal name for each page to match the namespace.

Is there a way to use namespace as the prefix on a set signal name, so that I don't have to enter each page manually, or a workaround that accomplishes this same goal? Similar to the behaviour of "Advanced Checkpoint with Namespace", I want to implement a "Setpoint with Namespace". It would make my life just a little easier  :)


Hoping for help! Thanks!

~D

Offline davidNeedsHelp

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +2/-0
Re: Is there a method to use namespace in set value signal names?
« Reply #1 on: September 12, 2025, 07:32:23 PM »
(Solved it, answering my own question here :) haha)


Hey user who I don't know personally!


What a great question! You must be quite the inquisitive (and probably pretty fun) individual!

If you read the manual (as you should always do before reaching out to a message board :(), you can find "Cloud Set Value". Using this component, and leaving the cloud connection parameter set to false, serves the same purpose as a regular set parameter, with namespace tagged on the front.


Happy GUIDEing!

~D