Author Topic: DM1200T Displaying Licence PDF  (Read 10049 times)

Offline NickHankin

  • PLUS+1 Novice
  • *
  • Posts: 1
  • Karma: +0/-0
DM1200T Displaying Licence PDF
« on: October 03, 2025, 10:03:14 AM »
Hi,

I'm a very new user of Plus+1, this may be a really obvious solution.

I am programming a DM1200T to be used as a display for giving live sensor readings on a vehicle.

Whilst waiting for the screen to arrive, i developed the programming for a 430 screen and tested it. This is worked well.

I made the same program on the DM1200T template and when it arrived, i uploaded the program using the service tool and the file downloaded successfully. But the HMI is only showing the licence agreement PDF. I can scroll though it but that's all i have.

Am i missing something with the new type screens that i must do in the programming, or have i got a faulty unit?

Thank you, nick

Offline samuelhj

  • PLUS+1 Developer
  • ***
  • Posts: 48
  • Karma: +1/-0
Re: DM1200T Displaying Licence PDF
« Reply #1 on: October 05, 2025, 06:42:26 PM »
Been a while since I worked on a new project involving these displays, but if I recall correctly you need to delete the licence page within the main Application.