Author Topic: DM1000 TEXT LIST ISSUE  (Read 10275 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 225
  • Karma: +7/-0
DM1000 TEXT LIST ISSUE
« on: July 23, 2025, 12:00:54 AM »
Hi there,

this should be a simple task to do but so far it seems not to work.

Basically I want to have a text list on a screen

it should be as simple as this:
drag the text list on the screen
drag the text into the text list or on the properties of the text list select list definition and should load it up. well none of this works

on the old displays this feature did work just fine
I wonder what has changed

of course you need your index variable

how do you create your text list in the DM displays?

thank you


Offline Lukey

  • PLUS+1 Guru
  • *****
  • Posts: 107
  • Karma: +12/-1
Re: DM1000 TEXT LIST ISSUE
« Reply #1 on: July 23, 2025, 03:47:38 AM »
It would seem you are doing everything correct.

Have you got a screen shot to share?

There is no difference from the old to new displays when using the Vector-Based Screen Editor, unless you have been using the Classic Screen Editor i dont know how this differs

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 225
  • Karma: +7/-0
Re: DM1000 TEXT LIST ISSUE
« Reply #2 on: July 23, 2025, 05:06:36 AM »
Hey Lukey,

I figure out what to do, now it ahs to be at properties then new list, just importing the list does not work

anyway something odd is that for some reason it creates the text twice, see picture text_2 the first one text phaseloss  then I ahve the same text for 2 index ...

if I try to delete it sometimes it does not let me do it, i have to start over the text list

kind of head scratch