Author Topic: What's about DP610 c3p5 ground pin?  (Read 22096 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 367
  • Karma: +12/-0
    • Marbek Elektronik
What's about DP610 c3p5 ground pin?
« on: October 23, 2013, 05:44:58 PM »
Hi,
I can't find any information about ground pin RS232 (c3p5) on DP610.

Is it isloated from power ground ?

Thanks,
Bernd
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
Re: What's about DP610 c3p5 ground pin?
« Reply #1 on: October 29, 2013, 02:34:38 PM »
here the answer from helpdesk (Thanks for it):

It is not isolated from the power ground. It is included in the connector to make it possible to use a single cable for connection to the RS232. You would otherwise need to splice the GND from some other GND point which would be inconvenient.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung