Author Topic: CS10 M2M Connection  (Read 8090 times)

Offline SJones

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
CS10 M2M Connection
« on: March 30, 2026, 05:00:24 PM »
i have been using the CS10 to setup a CAN Wireless bridge for over a year and have not had many issues,  setup was generally pretty easy.  However, I am now setting up the M2M connection with the latest version 125 CS10 program that is factory installed and I can not get the two CS10 to connect.  Just wondering if anyone else is experiencing any issues with the new version and if you found any work arounds yet.    When scan the Wifi networks with the CS10 in station mode, I can find the other CS10 but when I enter the password and click connect, it does not connect.  Best guess I have as of now, is that it is a password issue. 


Offline G30RG3

  • PLUS+1 Expert
  • ****
  • Posts: 91
  • Karma: +4/-2
Re: CS10 M2M Connection
« Reply #1 on: March 30, 2026, 05:44:39 PM »
Disclaimer: I do not have the CS10's available to test any more, and am not sure if following was with the CS10's or the WS103's I used before.
To be able to connect a Wifi-Bridge, I needed to deactivate the bluetooth mode.

Offline ToPe

  • Administrator
  • PLUS+1 User
  • *
  • Posts: 5
  • Karma: +4/-0
Re: CS10 M2M Connection
« Reply #2 on: April 23, 2026, 02:25:44 PM »
Hi
It is recommended to configure the CS10v125, especially the password settings, via a Bluetooth or Wi-Fi connection.

A new feature of the v125 update is that some parameters can only be written via an Interlink connection. This means that configuration is only possible via Bluetooth or Wi-Fi. This is to prevent unauthorized access to your CAN bus and lock you out (European RED-DA regulation).

Please try changing the parameters via Bluetooth instead of using the CG150.