Author Topic: PVED-CC S7 ISOBUS not reacting to CAN commands  (Read 12575 times)

Offline roeiamit

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
PVED-CC S7 ISOBUS not reacting to CAN commands
« on: December 23, 2025, 08:19:22 AM »
I'm using PVED-CC 32 Series 7 ISOBUS - Part Number: 11231865
I can see it sending messages on the CAN with no errors:
"0CFE1585", "7D 7D 30 FF FF FF FF FF"
"18FECA85","00 FF 00 00 00 00 FF FF"
When I send the commands:
"0CFE3506", "7D 00 02 00 00 00 00 00" or "0CFE3506", "7D 00 01 00 00 00 00 00".
It's not reacting and not giving me error message.
When I'm connecting with Service Tool, I can change the node id, but seems like there is a problem, the device it connected but it's written offline (see the image).
Also when I go to the diagnostic page, it's showing that there is no active error.
Any suggestions?

Roei

Offline Lukey

  • PLUS+1 Guru
  • *****
  • Posts: 108
  • Karma: +12/-1
Re: PVED-CC S7 ISOBUS not reacting to CAN commands
« Reply #1 on: December 24, 2025, 01:15:25 AM »
Seems like an ID or connection issue,

I cant see any connected devices in your ECU List ?

Try scanning the system again to confirm connection to the coil.

Offline roeiamit

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Re: PVED-CC S7 ISOBUS not reacting to CAN commands
« Reply #2 on: December 24, 2025, 05:40:25 AM »
I can see it on the CAN.
Also the Service Tool detects it.
I can change configuration and node id.
Maybe my diagnostic files are wrong?
The CAN communication is stable and working

Offline drphil69

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: PVED-CC S7 ISOBUS not reacting to CAN commands
« Reply #3 on: June 04, 2026, 10:24:07 PM »
You are telling it to extend or retract but your command is wrong.

Byte 0 is the command.  0xFD = 253 which is reserved.  The max command allowed is 250.