Author Topic: Mouse Defaults  (Read 10749 times)

Offline Scott_MARL

  • PLUS+1 Developer
  • ***
  • Posts: 17
  • Karma: +0/-0
Mouse Defaults
« on: November 13, 2025, 07:06:18 PM »
I have to be missing something. New PC, so fresh install of Plus+1 Guide and I am trying to set it up to have all the defaults I am used to.
Guide 2025.2.3.6627

Keyboard defaults are set normally, but I cannot find the mouse defaults.
Left button- select/apply
Middle button- menu
Right button- Gesture xy is pan, top left is menu, bottom right is exit
Back/Forward - last page/forward page respectively
My custom buttons does not work any more (logitec mouse with a extra thumb button I can apply macros to)

What I am trying to do is change the right button to "Pan with Hand" by default.
I cannot find this option and the tool bar button that used to be available, is not.

Can someone point me in the right direction please.
MARL Technologies

Offline Lukey

  • PLUS+1 Guru
  • *****
  • Posts: 108
  • Karma: +12/-1
Re: Mouse Defaults
« Reply #1 on: November 13, 2025, 10:36:24 PM »
I dont know where to find the settings for the mouse, however If you still have your old PC you can export/import your settings.

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 210
  • Karma: +38/-3
Re: Mouse Defaults
« Reply #2 on: November 14, 2025, 09:04:18 AM »
In the bottom RH corner of the Guide window there is a hand icon (Pan With Hand). If it is highlighted the right mouse button pans. If it is not highlighted it should work as you describe.