Author Topic: Entering a string from a DM1200?  (Read 10621 times)

Offline drphil69

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Entering a string from a DM1200?
« on: June 16, 2025, 05:25:56 PM »
I'm new to strings in Plus+1.  Are there any examples of:
1. How to allow a user to enter a string from DM1200 display?
2. How to put a string on the DM1200 display?

1. I believe this can be accomplished using ASCII code from a touch keyboard, put the ascii into array, convert array to string... but then can the string be put on the screen?  Or does each character need to be ASCII in order to put the characters on the screen (basically the 'old' way)?  Or, is there a direct way to have a user enter a string from screen using a touch keyboard?
2.  Is there a way to connect a string variable to the screen editor and display the string?  Any examples would be greatly appreciated!

Thanks,
Phil

Offline Lukey

  • PLUS+1 Guru
  • *****
  • Posts: 108
  • Karma: +12/-1
Re: Entering a string from a DM1200?
« Reply #1 on: June 18, 2025, 12:38:17 AM »
The DM1000 Application Example that can be downloaded from the update center will give you some good insight.

Yes you can send/display strings to and from the screen editor.
The keyboard from the DM1000 example outputs the value as a string, so that is a good starting point.