PLUS+1 User Forum
		PLUS+1 Hardware => Controllers => Topic started by: ET on June 18, 2012, 05:55:40 PM
		
			
			- 
				I'm currently programming/testing a MC050-10.
 It's hooked up to a 24 volt power supply for testing, and will be hooked up to a 24 volt system on the final machine.
 (Volt meter reads 24.07 V for the power supply.)
 According to the documentation, the digital outputs should be providing a voltage between 23 and 24 volts.
 However, they are only reading 10.23 V.
 I am able to accurately set the multi-function output pins to any voltage between 0 V and 24 V.
 
 How can I get the digital output pins to put out 24 volts?
- 
				Which pin are you exactly using?
			
- 
				Was using pins 31-36 on a MC50-10.
 Found out that they do work, but they were being turned on/off very quickly, approximating a PWM, giving the measured voltages.
- 
				You're right. The controllers doesn't have a ratiometric voltage output.
 If I need a "clean" DC voltage for e.g. a drive sensor or a constant voltage (12V supply for devices,...), I put a RC network (1k, 10u) at the output.