PLUS+1 User Forum

PLUS+1 Hardware => PLUS+1 Compliant Hardware => Topic started by: Marbek_Elektronik on August 06, 2026, 11:16:11 AM

Title: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Marbek_Elektronik on August 06, 2026, 11:16:11 AM
Hello,

there are al ot of PROF1 in the field.
And some of them may be defect after a long time of life.
But the PROF1 Joystick is out of production.
The JS1H joystick is the next one.
But the communication is not the same.
So what can users do?

What do you think about an adapter to simulate the PROF1
with JS1H ?
Does anybody have done this?
Perhaps, if not, I will think about it, do programm an Adapter with an Danfoss Controller like MC024 or an Display.
Title: Re: Adapter to simulate Prof1 with a JS1H Joystick ?
Post by: Rem on August 07, 2026, 02:18:22 PM
Hello,
Are your Prof1 joysticks identical?
There are many different configurations, particularly when it comes to communication. Are your Prof1s CAN-based?
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Marbek_Elektronik on August 08, 2026, 09:35:18 AM
yes, they are CAN-based.
I have add this information in the headline.
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Rem on August 10, 2026, 08:16:11 AM
Hello,
Why not modify the machine controller's program?
One option would be to use a parameter to select the type of manipulator.
Otherwise, an MC012 will suffice.
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Marbek_Elektronik on August 10, 2026, 08:59:52 AM
Because this software is not from me an sometimes no danfoss controllers.

MC012 has only one CAN port. I think, I need 2 of them, MC024-130 for example.
And then read the signals from JS1H and send it as protocol from Prof1.

Is this the solution? And has anyone her done this and can share the code?
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: G30RG3 on August 11, 2026, 02:20:16 PM
Hi Marbek_Elektronik,

I would go for a programmable JS1H, where you can recreate the messages (Option P2H in the modelcode).

Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Marbek_Elektronik on August 11, 2026, 03:11:35 PM
Hi "G30RG3",
we have this:
JS1H-XY-CJH-S-C33-TPR2-R-P1A-NNN-P1A-NNN-Y1A-NNN-Y1A-Y1A-Y1A-Y1A-NNN
Y1A-BRHN-NN

What do you mean with "P2H in the modelcode" ?

Is it possible to configure the JS1H CAN -Joystick, so the user sees a Prof1 Joystick?
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Lukey on August 12, 2026, 03:49:47 AM
Yes instead of JS1H-XY-CJH
Mode code would be JS1H-XY-PWH or JS1H-XY-P2H

PWH = PLUS+1® GUIDE Programmable PWM, Hall effect
P2H = PLUS+1® GUIDE Programmable PVE, Hall effect

This model code is basically a MC012 internally.
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Marbek_Elektronik on August 12, 2026, 02:13:55 PM
Do you think, we speak about the same problem?
I don't understand, what you mean.

My customer has a Joystik Prof1 CAN.
Now, I will give him a JS1H CAN.
But the protokoll doesn't match.
How can I configure the JS1H so, that it works like a Prof1 CAN?
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Rem on August 12, 2026, 03:49:58 PM
Hello,
What @Lukey means is that his joysticks are programmable.
So you can create a project using the joystick hardware:
(https://i.postimg.cc/670QNh8k/2026-08-12-15-43-23-Create-New-Project.png) (https://postimg.cc/670QNh8k)
(https://i.postimg.cc/y36QbsMH/2026-08-12-15-54-55-Clipboard.png) (https://postimg.cc/y36QbsMH)

Then you'll be able to interface it with your machine. 😉
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Marbek_Elektronik on August 12, 2026, 05:44:18 PM
Ah-Ok, Thanks...
But this doesn't solve the problem.
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: G30RG3 on August 12, 2026, 06:36:31 PM
Hi,
Sure Both the PWH and P2H can be programmed at will.
JS1H-XY-P2H-S-NNN-TPR2-R-P1A-NNN-P1A-NNN-Y1A-NNN-Y1A-Y1A-Y1A-Y1A-NNN-Y1A-BRLN-NN 
or
JS1H-XY-PWH-S-NNN-TPR2-R-P1H-NNN-P1H-NNN-Y1H-NNN-Y1H-Y1H-Y1H-Y1H-NNN-Y1H-BRWN-NN
would be a close match

It doesn't solve your problem, but maybe contact the helpdesk/Danfoss.  They might have got a package with the software pre-written.
I would expect Danfoss to have a compatibility solution for issues like these.   The last NN could be replaced with something else to get the compatibility you want.

It's bad enough that they forgot to keep the mounting holes compatible.
The 2 mm should not have made the difference.

Writing a MC24-130 to interface will also take a lot of effort, and is expensive (extra wiring, hardware, points of failure...)
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Lukey on August 13, 2026, 10:33:22 AM
My understanding is that your Joystik Prof1 CAN sends CAN messages to some other controller.

A JS1H PWH and P2H is GUIDE programmable and has a CANBUS connection, therefor you can program the in GUIDE to send the same messages like the Joystik Prof1 CAN
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Marbek_Elektronik on August 14, 2026, 10:04:16 AM
Ok, thanks, I will check this!
Yes it ist sending with address 1E4 or 1E6 (left/right) all 20ms the data.
Of course we can programm this messages.
I will try it.
Tanks again!
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: G30RG3 on August 31, 2026, 01:51:32 PM
What does the data look like in those messages?
Is there safety communication, besides the data in normal operation?
Title: Re: Adapter to simulate CAN based Prof1 with a JS1H Joystick ?
Post by: Marbek_Elektronik on August 31, 2026, 09:30:28 PM
No, only the proportional value is send.
At the moment I have another project.
When I work again with this joystick, I will send you the data I have logged.