PLUS+1 User Forum
PLUS+1 Hardware => PLUS+1 Compliant Hardware => Topic started by: roeiamit on December 23, 2025, 08:19:22 AM
-
I'm using PVED-CC 32 Series 7 ISOBUS - Part Number: 11231865
I can see it sending messages on the CAN with no errors:
"0CFE1585", "7D 7D 30 FF FF FF FF FF"
"18FECA85","00 FF 00 00 00 00 FF FF"
When I send the commands:
"0CFE3506", "7D 00 02 00 00 00 00 00" or "0CFE3506", "7D 00 01 00 00 00 00 00".
It's not reacting and not giving me error message.
When I'm connecting with Service Tool, I can change the node id, but seems like there is a problem, the device it connected but it's written offline (see the image).
Also when I go to the diagnostic page, it's showing that there is no active error.
Any suggestions?
Roei
-
Seems like an ID or connection issue,
I cant see any connected devices in your ECU List ?
Try scanning the system again to confirm connection to the coil.
-
I can see it on the CAN.
Also the Service Tool detects it.
I can change configuration and node id.
Maybe my diagnostic files are wrong?
The CAN communication is stable and working
-
You are telling it to extend or retract but your command is wrong.
Byte 0 is the command. 0xFD = 253 which is reserved. The max command allowed is 250.