PLUS+1 User Forum
PLUS+1 Hardware => Controllers => Topic started by: Rem on November 13, 2024, 12:16:08 PM
-
Hello,
We need to add functionality to a second-hand machine equipped with an OX24-110 module.
The number of outputs available to control a PVE coil is insufficient.
I'd like to know if it's possible to control two PVE coils simultaneously with a single output. Have you ever done this?
Thanks in advance.
-
PVE Ratiometric coils?
I have not physically tried it but in theory it should work just fine, the output from the expansion module is only a reference voltage to the coil/s, there is no load, there shouldn't be an issue.
-
We use active PVEA.
Thanks
-
PVEA is Ratiometric yes, therefor I would bet Yes it should work fine with two coils on 1 output.
Regarding Active feedback or passive that shouldn't be a concern as is only related to the Fault Output of the PVE to Input of Controller.
-
Thank you for your answers.
Have a nice day!
-
it is allowed to drive 3 PVEs on digitlal Power Output.
PWM Signal output is no problem.