PLUS+1 User Forum
PLUS+1 Hardware => Displays => Topic started by: george on November 04, 2024, 04:00:42 PM
-
Hello,
With the Plus+1 trial license I could flash and reflash a test application into the DM430E-0-0-0-0 display.
When the trial license expired, I switched to an express license and since then I am facing issues in reflashing the display.
I am not sure I am missing any additional project settings in my project configuration.
Could you please help?
The display is connected through the host PC using PCAN hardware with RP1210C driver.
Refer "Screenshot_1.png" for the gateway configuration.
Refer "Screenshot_2.png" for the system scan that recognised the display device.
Refer "Screenshot_3.png" for download file to ecu.
Thank you very much in advance.
-
Any thoughts?
This is a stopping issue and I am unable to get it resolved.
Is there any technical team I can talk to or an email where I can email the issue further?
Thanks.
-
You can reach out to the helpdesk if you have any issues:
https://www.danfoss.com/en/campaigns/dps/plusplus1-support-form/
Make sure you only have 1 display connected with the same Node ID. If you have more than 1 unit with the same Node ID connected you can get this error.
Also make sure you have the CAN terminated properly with 120ohm in both ends of the bus.
-
Thank you sverreo for your suggestion. It helped to re-flash the display.
I didn't realise I need to add a third node on the system in order to complete the flash sequence as per Screenshot_4.png.
I added a second PEAK hardware with a different device ID and it allowed me to complete the flashing.
I will write a detailed instruction later for the benefit of others.