PLUS+1 User Forum
		PLUS+1 Tools => PLUS+1 GUIDE => Topic started by: Marbek_Elektronik on October 02, 2020, 01:56:24 PM
		
			
			- 
				Hi,
 I place a port in Guide page interface editor, OK.
 If I want to place a second port, I can't edit the name while I am placing it.
 Is there a key combination?
 
 Today I place the second port an press "Esc" and then press "Q" and then edit this last port.
 
 Is there a trick?
- 
				Hi Marbek_Elektronik,
 
 I see what you mean, you would like to have the "Entry attribute" pop-up every time you place a port, and not every time you click "Wire/Bus Port"?
 Now it adds a number to the end of the name you choose for the first one, like port, port1, port2 and you need to manually change the name.
 I believe that you usually have different names on ports, so it would be logical to have the attribute pop-up every time you place the port.  I will ask the developers about this.
 
 What you can do is clicking the "Wire/Bus Port" button every time, then the attribute pop-ups before you place it. You don't have to press "Esc" until you are done.
 
 Have a nice day.
 
 
- 
				Yes, thanks.
 
 Another thing is placing constants:
 It would be very nice, if the value popups after placing it.
 At the time, I place it and then type "Q" and edit it.
 
 
- 
				Hi,
 
 I had the "constant" discussion with my colleague as well and I will absolutely bring this up.
 
 
 Have a nice day.