PLUS+1 User Forum
		PLUS+1 Software => Communication => Topic started by: Beezkneez on January 21, 2020, 12:03:32 AM
		
			
			- 
				Hello,
 
 I've searched the forum and saw a few other threads that are fairly similar but did not see any real evidence of people using Ethernet/CAN bus converters. Has anyone done this or had success at this? I've found a few online but would be interested to know if someone is already doing this and if they had any recommendations.
 
 I am looking to receive receive TCP/IP data packets and convert them into CAN messages.
 
 Thanks in advance!
- 
				Hello,
 
 I don't know of anything that is already in existence (with the exception of another brands controller), but I do know what is possible in regards to development boards, you could use a Raspberry Pi, or Clicker 2 board from Mikroelectronica could be a neat solution loaded with an ethernet click and a CAN click.
 
 https://www.mikroe.com/clicker-2-pic18fj
 
 I have used the Clicker 2 in a couple of applications (including the CAN click) and it's a cool thing.
 
 Cheers,
 
 John.
 
- 
				Had to look into it for a similar project and was recommended something along these lines. I haven't used them sorry, I don't know how easy they are to use.
 
 https://www.anybus.com/products/gateway-index/anybus-xgateway/detail/anybus-x-gateway-ethernet-adpater-server-j1939
 
- 
				hey,
 
 I have used modbus to Can gateways, one from EATON, with this you have to write down the code and you have to understand both comm protocol otherwise becomes a headache. after all it did work fine.
 the last one I used was from Pyramid technologies and it was modbus to J1939 for hazardous locations, this is really nice simple to use it is a little price because of the certs
 
 I do have some from anybus  but for some reason I did not make it work, have not tried anymore but the key is to understand both comm protocols, for sure you undestand CAN.
 
 I hope this helps
- 
				Thank you, all! I will be looking into all of those leads this morning. Really appreciate it!
			
- 
				Try a wago 750-658, I use this on a regular basis.
 The module is limited 48 bytes, if you need more, add another wago module.