Author Topic: Red is not Red after Guide 11.1.5  (Read 2467 times)

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Red is not Red after Guide 11.1.5
« on: December 21, 2023, 10:09:13 PM »
It is an old problem and I am still working with Guide 11.1.5 because of this.
Now I must work with the newest version because of svg files and bugfixes of course.

The contrast in dark mode between red/black and between green/black (bus, wire) is not the same as before.
I can't work well.

Red is not 0xFF0000, it is now 0xF03658 !

Please compare the old color schema with the new one.

Can I change anything in options in Guide or in Windows ?
« Last Edit: December 21, 2023, 10:11:31 PM by Marbek_Elektronik »
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Red is not Red after Guide 11.1.5
« Reply #1 on: December 22, 2023, 12:19:03 PM »
Please, can someone tell me the color-values of red and green (bus, wire) in Guide 2023 ?
You can use a color tool.
I have used "ColorPicker". There are a lot of    tools, which can do this.

In my Guide red is only 0xF03658 and not 0xFF0000, so contrast is not good.

Thanks!
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung

Offline Matt_Eng

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +10/-0
Re: Red is not Red after Guide 11.1.5
« Reply #2 on: January 02, 2024, 05:36:57 PM »
Hi,

These are the colors I get in 2023
Red : 0xf03658
Green: 0x1ad55f

The muted colors took me a bit to get used to as well. There is a way to make them vibrant with a built in tool of Windows.
In the start menu if you search "Color Filters" you'll get some accessibility options that can be helpful.
 I've found that the "Red-green (green weak, deuteranopia)" option can help boost the red and green to get them back to the former vibrancy.

-Matt_Eng

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: Red is not Red after Guide 11.1.5
« Reply #3 on: January 04, 2024, 02:41:32 PM »
Thanks,
I will try this workaround.

At the moment I use the white background. Here the color is OK. It would also be nice, we were able to set the color.

My monitor is 30" and 3840 × 2160 Pixels.
Here, the green wires are very small, you have to search them.

It would be nice, if we coud choose the thickness.

I think Danfoss has developed Guide for Laptops.
But there are also 30" monitors.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung