PLUS+1 Software > Displays
Text not formatting properly
(1/1)
dlewis:
I'm using a DP710 and Guide 9.0.7. I'm having an issue with text formatting properly on the display screen. When I view the text within Guide, it shows the proper formatting, but when I compile and download it to the display, the display does not have the same format. I don't remember having this issue in previous versions of Guide.
oiltronic:
What aspect of the format is incorrect?
Nilla:
Hi dlewis!
What is your setting for the screen resolution on your computer? Having e.g. it set to 125% at compilation in GUIDE could give this behaviour after download to a display. There actually is a requirement in the Release notes for GUIDE that you need to use Display/text size set to 100% at all times.
Best regards
Nilla
PLUS+1 Helpdesk
dlewis:
It is removing blank lines between text lines. In another instance, it combined multiple lines into one. My screen is at 100% with a resolution of 1920x1080.
Nilla:
Hi dlewis!
I've done a simple application for a DP710 adding some text with blank lines as both a simple text and also in a text list, see attached, but I'm not able to replicate what I think your issue was based on what you stated above. Tried out a blank line both with and without any space on it. Would you be able to send us your application in a .P1P-format to plus+1helpdesk@danfoss.com so I can have a look at it and trying to download it on my testbench?
Best regards
Nilla
PLUS+1 Helpdesk
Navigation
[0] Message Index
Go to full version