PLUS+1 Software > General controls
Internal Coils
paterianus:
It's called a bus port (the yellow oval with a line above and below) and you could name one "internals" to emulate internal coils.
Mike Stiffler:
Hello:
OK, I'll give that a try.
Thank you,
Mike
bgtwuk:
Hey Mike
Have you got your internal bits working?
Bgtwuk
Mike Stiffler:
Bgtwuk:
No, I'm not sure how to do it.
I tried one idea with some test code and it would not compile.
If you have any additional information or an example, it would be nice.
Thank you,
Mike
Mike Stiffler:
Hello:
I was able to create a new bus called Man_Mode, write a variable to it via some Boolean logic using the variable name Man_Mode_Enabled, and then latch a logic circuit from that new bus with the Man_Mode_Enabled variable as an input. The code compiled with no errors.
Now I need a way to test the code to see if it will work. I have a breakout board but have not wired it yet. Is there a way to force the input on and simulate the MC24-20 microcontroller running to test the code? Is it possible for the service tool to do this? I've got the feeling that I'll have to wait untill I can wire it to the breakout board to test the code. Any other suggestions?
I feel I'm making some progress.
Thank you,
Mike
Navigation
[0] Message Index
[#] Next page
[*] Previous page
Go to full version