Author Topic: Rotate Text  (Read 1641 times)

Offline dlewis

  • PLUS+1 Guru
  • *****
  • Posts: 103
  • Karma: +2/-0
    • Getman Corporation
Rotate Text
« on: February 08, 2024, 05:27:51 PM »
I would like to use a DP720 in a portrait orientation rather than Lanscape.   Rotating any graphics is not an issue, but how do I rotate text?  There are even times when I'm using the display in the normal orientation in which it would be nice to rotate the text.

Any ideas, besides importing the text as a graphic?

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +3/-0
Re: Rotate Text
« Reply #1 on: February 09, 2024, 01:33:20 AM »
I've been searching for an answer to this too. Importing as a graphic only works if the text is static. If it varies, as in supply volts, that won't work.

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +3/-0
Re: Rotate Text
« Reply #2 on: February 09, 2024, 01:40:58 AM »
HaHa found it. See attached screen shot and other thread. (https://www.plus1forum.danfoss.com/index.php?topic=871.msg3570#msg3570)