PLUS+1 Software > General controls
Electric Motors & VFDs
(1/1)
metalninjadragon:
I recently got a project to develop an interface to a variable frequency drive for a complex system
(I can't tell you what but it is not an HVAC or water treatment application)
I know Danfoss has a line of VFD's is there any integration with the Plus+1 environment.
Ideally, I'd like work in this environment to maintain compatibility with some of our other products, but I'm kind of nervous about tackling CANOpen protocols in Guide, I think I might need a more traditional C environment for that.
thoughts? has anyone else been down this road?
oiltronic:
I didn't know that Danfoss makes VFD's, but I do know that there is no integration with the Plus+1 environment. Plus+1 is targeted for mobile hydraulic machinery, usually far away from the land of VFD's. I'm sure the two Danfoss divisions have never met, let alone tried to integrate things.
I program in C as well as the Plus+1 environment, and making reliable custom CANOpen communications is actually pretty fast & easy in Plus+1. Drawing the 'code' to pack & unpack all the flags and data can certainly get tedious though.
hgb1992:
Hello!
Sry for the late reply. But probably this can help:
Schwarzmüller Inverter (member of Danfoss PS Group) offers Inverter (low voltage Level VFD's for mobile applications).
This Inverters are fully programmable with PLUS+1 GUIDE.
Kind regards, Benedikt
dlewis:
It would be nice if Danfoss would make a driver of some type that could feed into a off the shelf high voltage VFD 8). Even in mobile systems, I still use high voltage motors.
swordfeather:
Hi,
In a project we are using the Schwarzmuller MI08 inverter.
I was not able to find the Schwarmuller hardware file on update center.
Anyone has a link for this file?
Greetings
Navigation
[0] Message Index
Go to full version