Author Topic: ExecTimeWork ?????  (Read 2376 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 113
  • Karma: +1/-0
ExecTimeWork ?????
« on: March 08, 2022, 11:41:29 PM »
Hi!

I use DM430E I use check point to see ExecTime,  ExecTimeGraph and ExecTimeWork but this last I can see it.
Please could you tell if ExecTimeWork is watching.  If yes Please show me how can I see it.

thanks in advance
Cordially
mac Bahi

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: ExecTimeWork ?????
« Reply #1 on: March 09, 2022, 07:02:23 AM »
Hello mac Bahi,

See attached image, it explains it a little better than I can.
This is taken from the DM1000 API specification, but I believe it works the same for the DM430E.
If you want even more information you can open the DM1x00 API from the hardware tab in PLUS+1 GUIDE (If you have the DM1x00 install that is), and search for "Main and Background Tasks".  There are some very useful information.

I hope it helps.
« Last Edit: March 09, 2022, 07:06:59 AM by Tor »
Best regards,
Tor
PLUS+1® SW PAE Team