Author Topic: Danfoss temperature sensor in Plus+1 Service Tool  (Read 9855 times)

Offline deyan.dimitro

  • PLUS+1 Novice
  • *
  • Posts: 3
  • Karma: +0/-0
Danfoss temperature sensor in Plus+1 Service Tool
« on: January 16, 2019, 12:43:27 PM »
Hello,

i have a temperature sensor connected in ECU. Input pin is C1p27.Ohm and unit is Ohm. I must not change nothing in GUIDE Project File.

Can i get the information from this pin but in degrees in Service Tool?
I have Danfoss temperature sensor table.

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: Danfoss temperature sensor in Plus+1 Service Tool
« Reply #1 on: January 24, 2019, 08:46:29 PM »
No, not really.  All the elements only offer linear scaling, some with an offset.  I can think of two options:
  • Insert that image into the service tool for manual ohms-temperature cross-referencing, or
  • break the table into sections that are nearly linear, within your tolerance, and put in "panel" objects for each of the ranges, using the "hide component" feature to select a valid range of ohms for which to display the particular panel.  Then insert a linearly converted standard log object in each panel for that range.