Author Topic: image background  (Read 2887 times)

Offline topal

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +0/-0
image background
« on: June 04, 2019, 08:08:41 PM »
Hello everyone

I am new on the forum and like all the new ones I have a lot of questions because even after having read and reread the PLUS1 GUIDE User Manual in-US there are things that I do not understand then I start

in the bus to do a simple trick, I would just like to display an immage on the screen of my DP250, but I do not understand the logic, could you help me understand how to display a picture of func on the screen

thank you in advance

Pat

Offline oiltronic

  • PLUS+1 Guru
  • *****
  • Posts: 170
  • Karma: +15/-0
Re: image background
« Reply #1 on: June 06, 2019, 05:17:49 PM »
What GUIDE version are you using? 
Classic or Vector-based screen editor?
How far have you gotten, and where exactly are you getting stuck? 
Are you unable to import an image?
Or are you having trouble with the logic to selectively turn on & off the image in the program?

See also the "Screen Editors" section of the user manual (GUIDE menu item Help->User Manual), in particular search for "Edit Image Window".

Offline Jakob

  • PLUS+1 Expert
  • ****
  • Posts: 98
  • Karma: +2/-0
Re: image background
« Reply #2 on: June 07, 2019, 03:41:43 PM »
All the DP250's I have seen only run in the classic editor mode.
So first thing you need to do is to setup the display area, then you can start designing what you want shown on the screen.
Which is done by Importing images, creating text, that you then am able to drag into the screen area.

And then you can enable what images/text/display areas that you want shown.

Offline topal

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +0/-0
Re: image background
« Reply #3 on: June 07, 2019, 10:23:32 PM »
Hello,

good explications, now i can display images and texts on my first page

i'm happy

thank you

Pat