Author Topic: Sc024-120-C1P10 with joystick APEM  (Read 12091 times)

Offline macbahi

  • PLUS+1 Guru
  • *****
  • Posts: 127
  • Karma: +1/-0
Sc024-120-C1P10 with joystick APEM
« on: October 08, 2024, 11:30:21 PM »
Hello,

I use Sc024-120 input C1p10  with APEM joystick TS6A1P00A  use 5 Volt.

The joystick is Hall effect technology.  It has 2 axis and one push button.

I connected it to C1P08 (Snsr_Pwr  5V) and the ground is C1P09.

First axe is connected as C2P1 and push button is connected to C1P10.  The push button has ground configuration.

So my C1p10 bias is set to 1 as shown in image.

My problem is the push button don't work  but when I use my voltmeter I see the push button working.

Please Have you idea what is my problem.

Thanks in advance for your help.

With best regards

Offline sverreo

  • PLUS+1 Developer
  • ***
  • Posts: 21
  • Karma: +1/-0
Re: Sc024-120-C1P10 with joystick APEM
« Reply #1 on: October 09, 2024, 01:17:00 PM »
Have you checked the voltage on the input in ServiceTool?

Voltage should be 5000mV and DigIn=0 when the button is off, and 0mV and DigIn=1 when the button is pushed.