Author Topic: S42 EDC hardware template not putting voltage on pin.  (Read 4878 times)

ET

  • Guest
S42 EDC hardware template not putting voltage on pin.
« on: June 20, 2012, 09:45:08 PM »
To simplify the programming of my MC050-10, I'm using the hardware template for the S42 EDC pump, located here:
http://www.sauer-danfoss.com/Products/MobileElectronics/PLUS1Guide/PLUS1GuideDownloads/PLUS1ComplianceBlocks/index.htm

I've hooked up the necessary buses and input signals, and set it to +50% output (i.e. 5000 on the CmdIn wire).
However, the two pins allocated (44 and 45) have zero voltage on them.
I know I can set the voltage or amperage myself, as I have put pin 42 on a PWM with 50% output.

What should I investigate to get this working?

Offline BRIan

  • PLUS+1 Expert
  • ****
  • Posts: 56
  • Karma: +3/-0
Re: S42 EDC hardware template not putting voltage on pin.
« Reply #1 on: June 20, 2012, 11:22:11 PM »
Have you got the EDC or dummy resister connected? EDC blocks shut down if resistance is too high or too low.

ET

  • Guest
Re: S42 EDC hardware template not putting voltage on pin.
« Reply #2 on: June 20, 2012, 11:29:44 PM »
I have neither connected.
I assume I need a 18/20 ohm resistor to simulate the two coils?
I can't recall where I managed to find that, but I'm pretty sure that's what the docs said the resistances of the coils were.

ET

  • Guest
Re: S42 EDC hardware template not putting voltage on pin.
« Reply #3 on: June 21, 2012, 07:34:44 PM »
Works with a 19 Ohm resistor on each pin.