Author Topic: DM1000 CHART  (Read 3500 times)

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
DM1000 CHART
« on: November 26, 2021, 02:52:43 PM »
Hello Guys,

has anyone have done something like this with the DM1XXX?

- showing numeric values and plot of trend of the variables- line graph variable versus time-

basically something like what is done in a spreadsheet, you have your data and you make a plot of the behavior overtime

if so what was the trick for that?

or do you know any other display that could do that?

thanks for the advise

Offline Nickyk

  • PLUS+1 User
  • **
  • Posts: 5
  • Karma: +1/-0
    • Hydrauvision
Re: DM1000 CHART
« Reply #1 on: December 13, 2023, 01:58:22 PM »
Hey Pinias,

I'm looking into doing something similar in a DM1200T. Did you in the meantime figure something out to do this?

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: DM1000 CHART
« Reply #2 on: December 19, 2023, 02:06:29 PM »
Hey Nickyk,

I gave up on that with the DM1000, I did not find out a way to do that.

I have to switch to a different display -X2 10 inches-

for my application it was not that bad, the controller does all the logic and the display is just that,  a display to monitor all parameters, the other benefit on this display is that it can log to a stick memory  so the memory limitation for logging is not a bad thing. it can do screen shots.

I hope this helps
Regards

Offline Marbek_Elektronik

  • PLUS+1 Guru
  • *****
  • Posts: 351
  • Karma: +8/-0
    • Marbek Elektronik
Re: DM1000 CHART
« Reply #3 on: December 21, 2023, 07:27:43 PM »
I also want to do this next weeks on DM430E.
If it is ready, I will post it here.
Marbek Elektronik, Dipl.-Ing. Bernd Konrad
Dienstleistung, Entwicklung, Herstellung