Recent Posts

Pages: 1 ... 6 7 [8] 9 10
71
Displays / Re: Changing image size in program? vector editor
« Last post by Marbek_Elektronik on March 14, 2024, 09:35:52 PM »
Oh, it would be fine, if I find a turorial about this.
I am just reading the manual about widgets.
72
Communication / Re: Communication
« Last post by AP on March 14, 2024, 01:38:24 PM »
here is the Rx code used to receive data.
73
Communication / Communication
« Last post by AP on March 14, 2024, 01:37:30 PM »
Hello, I am new to Danfoss.

Trying to transmit and receive data from controller (MC023-120) to display (DP710), eventually display the data received from the sensor.

What am I supposed to do?

I just want to send a raw mV value.
74
Displays / Re: Changing image size in program? vector editor
« Last post by Lukey on March 14, 2024, 12:08:55 AM »
My second image is the Widget properties, you can input a signal from your program to control the Width and Height of the signal.

These can be used to adjust the size in the program while running.
75
Displays / Re: Changing image size in program? vector editor
« Last post by Marbek_Elektronik on March 13, 2024, 10:00:47 PM »
Thanks,
but I don't understand your second image.

I don't find "signal input"
(it is svg format)
76
Displays / Re: Changing image size in program? vector editor
« Last post by Lukey on March 13, 2024, 02:44:23 PM »
I believe it is, I have not done/tested this exactly but I imagine you could create a text/image widget.
Set ScalePos and ScaleSize to True for the object in the Widget.
For the Widget property set the Width and Height externally with an input.

Some combination of the above should achieve the outcome.
77
Displays / Changing image size in program? vector editor
« Last post by Marbek_Elektronik on March 13, 2024, 12:57:46 PM »
Hi,
is it possible to change image size by running?

I want to change font size and image size by run-time.

Currently, I only know that this works before compiling and then the size is defined.

(Rotation ist possible, i know)
78
PLUS+1 GUIDE / Re: Missing fonts error when trying to compile with 2024.1
« Last post by williamk on March 06, 2024, 06:08:52 PM »
This appears to be fixed in 2024.1.4
79
Controllers / Re: Parameters not visible
« Last post by SVK on March 06, 2024, 01:42:51 PM »

I found what was wrong.
The OS was different, all parameters became visible when I updated the OS.

Thx for the help though.
80
Controllers / Re: Parameters not visible
« Last post by Tor on March 06, 2024, 08:25:09 AM »
Hello SVK,

If you open the service application in an earlier version of Service Tool does it work?
In that case I would recommend you to create a case for PLUS+1 Helpdesk:  https://www.danfoss.com/en/products/dps/software/software-and-tools/plus1-software/#tab-support

If there have been a name change for some reason, you need to open the service screens and change the signals to the correct ones. I have marked in the attached image where to look when using a regular parameter component in Service Tool.
If you don't have permission/access to do this, I would recommend you to contact the developer of the service screens or the machine manufacturer.

Have a nice day,
Pages: 1 ... 6 7 [8] 9 10