Author Topic: Conditional Hide Page  (Read 3758 times)

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 191
  • Karma: +36/-1
Conditional Hide Page
« on: September 26, 2022, 06:28:14 PM »
Does anyone know if it is possible to hide a log or parameter page based on a condition in a similar way to setting a hide condition for the visibility of a component? The only option I can see is Hide in Run Application Mode.

I was about to post it as a suggestion but thought I would check here first in case I am just missing it!

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 276
  • Karma: +27/-1
Re: Conditional Hide Page
« Reply #1 on: September 27, 2022, 09:12:21 AM »
Hello acmall,

Unfortunate no.
The closest thing is to use the hide functionality on a Panel component. This will still leave an empty page in your Parameter Page tree, but you only need to do the hide setting on one component, not 50.

This wish is already in the wishlist, so there might be a solution in the future.


Have a nice day.
Best regards,
Tor
PLUS+1® SW PAE Team

Offline acmall

  • PLUS+1 Guru
  • *****
  • Posts: 191
  • Karma: +36/-1
Re: Conditional Hide Page
« Reply #2 on: September 27, 2022, 09:48:54 AM »
Thanks for confirming Tor.