Author Topic: Display Outputs  (Read 6782 times)

radioact

  • Guest
Display Outputs
« on: November 18, 2010, 06:01:12 PM »
I know the DP610 display does not have signals intended as general purpose outputs, but I was wondering about the ratings of the pins for encoder power supply and the buzzer output. I read through the datasheet and I didn't see anywhere that specifies what the max current source is for C1P8, and the current sink of C1P12. Its just for my peace of mind that what I hookup to these output is not more then the screen can handle (Can I connect an air raid siren to the buzzer to get peoples attention? ;)).

Tyler

radioact

  • Guest
Re: Display Outputs
« Reply #1 on: November 18, 2010, 07:17:58 PM »
So I answered half my own question,

Well I was digging around in the outputs page an I found a note on the output C1P8 page that states max current is 400mA.

Now does anyone know the other half?

Tyler

Offline Stefan

  • Administrator
  • PLUS+1 Expert
  • *
  • Posts: 72
  • Karma: +0/-0
Re: Display Outputs
« Reply #2 on: January 31, 2011, 10:42:25 AM »
Hello,

Sorry for the late answer.

C1p12 can sink 0.5 A

Best regards
Stefan

BetterAdapted

  • Guest
Re: Display Outputs
« Reply #3 on: February 21, 2011, 11:16:18 AM »
note pin 12 does not have a back emf diode