Author Topic: Difference Between CAN 0 and CAN 1  (Read 7175 times)

jgarzon

  • Guest
Difference Between CAN 0 and CAN 1
« on: October 01, 2012, 06:45:53 PM »
Hello My Friends

Something I'm new at this and I have a question
What Is the Difference Between CAN 0 and CAN 1?

Thanks in advance for the clarification of my question

_________________________________________________-

Hola Mis Amigos

Soy Algo Nuevo En Esto Y Tengo Una Pregunta
¿Cual Es La Diferencia Entre El CAN 0 y CAN 1?

Gracias De Antemano Por La Aclaracion De Mi Pregunta

Offline hproffitt

  • PLUS+1 Developer
  • ***
  • Posts: 28
  • Karma: +0/-0
Re: Difference Between CAN 0 and CAN 1
« Reply #1 on: October 01, 2012, 07:15:46 PM »
The main difference that I am aware of is that you can only download a new .lhx file to CAN0.  Besides that, they are just two separate CAN channels that you are able to utilize to lower your bus load and/or separate functions that may interacting with a different location on the machine.