PLUS+1 User Forum
PLUS+1 Software => Communication => Topic started by: power4 on November 05, 2013, 10:33:22 PM
-
I am trying to connect a MC050 or MC024 controller to some motor controllers which are working as CANOpen Slave nodes on a CAN bus. The MC controller will be a CANOpen Master node, which needs to initialize the slaves and send TPDO message. I noticed the built-in CAN module in the controller is very generic, so, I just want to ask if there is a library or module directly for CAN master node.
Thanks.
-
Hi Power4.
no there isn't you have to build the logic into the controllers yourself.
I have succesfully run Danfoss FC electric motor drives from a DP610.
regards Neil.