Author Topic: Transmission output speed  (Read 6018 times)

Offline Mike AA

  • PLUS+1 Guru
  • *****
  • Posts: 109
  • Karma: +0/-0
    • Dewind Dewatering
Transmission output speed
« on: October 06, 2015, 07:19:45 PM »
I am now working on hooking up a speed sensor on an Allison 5 speed transmission output to my controller. I am using an Ai-Tek Instuments 70082-100-022 or -024 cant remember which model but they're the same specs. The PDF is http://www.aitekinstruments.com/wp-content/uploads/2012/08/Side-Look.pdf. I am using the dual coild but currently only hooked to one coil. I have this connected to C1P23 of MFC050-018, pinconfig0=0 pinconfig1 =1, diginconfighigh 300, diginonfiglow 200. The machine this is hooked to I currently don't have the ability to test but I am looking for input as to if these settings and my code will work? When I have the chance to test I wont have a lot of testing time so if I can get it running quicker with less changes would be great.

Thanks
-Mike