Author Topic: DP610LX USB host  (Read 5098 times)

Quax76

  • Guest
DP610LX USB host
« on: June 28, 2012, 03:50:17 PM »
Hi everybody,

has anyone tried to use the USB host interface on C3 from the DO6x0LX for App logging?
I didn't get any connection to the USB storage (stick).
+5V supply Voltage is OK.
I used the blocks from the new Display libary, but it doesn't seem to work.
On my stick, there is a status led. The led stays off.
When I use a CP to show the status of the "write_to_USB" block from SD the value stay at "0", even when no Srick is connected.
Do I have to define some new HW ports, which are not defined in the 70059412v100 template?
When controlling the C2p06_C3p07.Mode Value in the Service Tool, it contains "0", but in Guide, it's definitly "2".
Anyone out there who get this working?
THX,
Quax