Author Topic: Deleting a signal connected to a bus  (Read 3147 times)

Offline spittet

  • PLUS+1 Guru
  • *****
  • Posts: 117
  • Karma: +6/-1
Deleting a signal connected to a bus
« on: April 26, 2020, 10:31:21 PM »
Hi,

I noticed that I'm doing a lot of times a specific set of operations when I'm deleting a signal that is connected to a bus in GUIDE.

Here are some pictures of the process (see joined) :

A : Starting Point
B : After first delete step.
C : After second delete step.

To go from A to C, I do the following steps :

- Press "Delete" button on my keyboard.
- Select the signal lines, signal name and a portion of the bus in the same selecting box.
- In the "Select Item Class" prompt box, I choose "Toggle ON/OFF" and I toggle to OFF the "WireBusSegment". I press OK.
- Select the remaining signal lines in the same selecting box.

First, if there is a faster/easier way to achieve this end result, I would gladly would like to know about it.


Second, to me, I think it would be easier if we could only do a right-click on the junction (where the signal exits from the bus) and simply choose a "Disconnect from bus" option. This would remove the signal name and all the associated signal lines up to the next component connected to this signal line (or up to a junction to another signal line).

Additionnaly, you could do right-click on the signal line and you could choose between 2 options :

1- Unroute this segment : remove only this specific signal line
2- Unroute this signal : remove all signal lines related to this net/signalName

Have a good day!

Offline Tor

  • Administrator
  • PLUS+1 Guru
  • *
  • Posts: 275
  • Karma: +26/-1
Re: Deleting a signal connected to a bus
« Reply #1 on: April 27, 2020, 01:17:57 PM »
Hi,

I searched the PLUS+1 wish list but couldn't find anything like this.
Added to wish list as number W01167.
Best regards,
Tor
PLUS+1® SW PAE Team