Author Topic: Danfoss MC and Load cell  (Read 3528 times)

Offline Beezkneez

  • PLUS+1 Developer
  • ***
  • Posts: 45
  • Karma: +2/-0
    • Trebro Turf Equipment
Danfoss MC and Load cell
« on: March 08, 2019, 07:37:43 PM »
Has anyone successfully used a Danfoss Micro to measure an input from a load cell? The load cell in question is an Omega LC101-5K. The output from the Wheatstone bridge circuit is a very small mV signal and I am not sure how this can be read with a Danfoss controller. We are using an MC050-110.

Would an amplifier do the trick? Just curious if this has been done already and if so, what advice someone may have.

Offline jashom1

  • PLUS+1 Expert
  • ****
  • Posts: 78
  • Karma: +6/-0
Re: Danfoss MC and Load cell
« Reply #1 on: March 11, 2019, 10:52:49 PM »
Hi,

Have you seen this thread?

http://www.plus1forum.danfoss.com/index.php?topic=879.msg2672#msg2672

I haven't used them but they should work.

Cheers,

John.

Offline Beezkneez

  • PLUS+1 Developer
  • ***
  • Posts: 45
  • Karma: +2/-0
    • Trebro Turf Equipment
Re: Danfoss MC and Load cell
« Reply #2 on: March 12, 2019, 03:17:57 PM »
I did not see that thread. Thanks John.