PLUS+1 Hardware > Displays
DM430E/M - Replacing 1-1-x-x to 0-1-x-x display
samuelhj:
Hello all
I'm replacing a DM430M 1-1-x-x it was 0-1-1-x display for a DM430E 0-1-1-x 0-0-1-x display and I'm wondering the procedure to do so, by memory I thought I could just add the new hardware to the Plus1 program but I can't seem to figure it out.
Anyone who has done something similar?
Edited post to correct for version of the displays.
BRIan:
Either use Compare SCS files... in the Tools menu to see the differences of blank applications, or compile it and it will tell you where you have missing or extra components.
Lukey:
Yes it's simple go to the Hardware, right click and select "Use this hardware in project"
Them compile and GUIDE will tell you if there is any issues, I only expect there would be issues if you've used some of the features of the old hardware that being the 2nd CAN port and the USB/RS232
samuelhj:
Thank you for the reply.
I assume you're talking about the HWD menu in Guide? I only see a method of updating to latest hardware version. I already have the correct hardware version installed via the update centre, and i can create a new project, but I can't seem to figure out how I convert my older program to the other hardware version.
Even if I add the module to the new project, and attempt to compile, I get the error "Unable to compile project due to invalid search database."
Pardon my ignorance, I haven't had to deal with going from one hardware type to another before.
Tor:
Hello,
Maybe this YouTube video can help you?
https://youtu.be/ux4LifGHkwI?si=8fDxCjalYLZ5hVeI
Have a nice day.
Navigation
[0] Message Index
[#] Next page
Go to full version