PLUS+1 Software > Displays
Page areas
(1/1)
tjozmin:
I am trying to set page area that I can use for alarms and indicators. I want this to be shown on top of most pages but not all. Regardless of teh order it is only shown on the first page. When I change pages it gets hidden. If this has the highest order shouldn't this always be on top. Do I need to enable this area after every page change?
Niska:
Yes, unfortunately you have to trig a new activation for getting your alarm area at top.
Richard:
Hi tjozmin
The way I achieve this is to set port colours to transparent on the screens where I want to see the warning area and use a full size background image with a transparent window so that the warning icons are visible through it. I found this method the most simple as it does not involve re-enabling ports in some screens and not others. The warning port can also be enable full time with True rather than more complex control logic. I never use priorities and only use order for images within a page.
Richard
Navigation
[0] Message Index
Go to full version