Author Topic: Serial communication RS232 with DP600  (Read 6747 times)

Pascal

  • Guest
Serial communication RS232 with DP600
« on: June 11, 2012, 05:28:15 PM »
Hello,
I have to receive data from PLC by RS232 (only available) and on my machine I have DP600 so I think it's possible to do it with C3 rear plug !
Anybody already programmed blocks to receive data by RS232 port ?

I have to search characters inside data, I think i have to play with ARRAY ???

Thank you.
If you could answer in French ... no problem  :)
« Last Edit: June 11, 2012, 05:43:58 PM by Pascal »

Offline Neil

  • PLUS+1 Expert
  • ****
  • Posts: 96
  • Karma: +2/-0
Re: Serial communication RS232 with DP600
« Reply #1 on: June 11, 2012, 08:42:55 PM »
Bonjour Pascal,

envoyez-moi votre email et je vous enverrai ce que j'ai fait.

 merci Neil

Thomas

  • Guest
Re: Serial communication RS232 with DP600
« Reply #2 on: June 12, 2012, 01:45:03 PM »
Hi!

Here is an example if it can help you in any way.

Best regards // Thomas

Offline pinias

  • PLUS+1 Guru
  • *****
  • Posts: 215
  • Karma: +7/-0
Re: Serial communication RS232 with DP600
« Reply #3 on: April 17, 2013, 04:16:58 PM »
Hello Sthepan,

The rs232 file is for a DP610 display however the DP600 has the rs232 port also, the problem that I have is that if I look for the rs232bois bus it is not there.

What do I have to do in order to be able to choose the RS232 bios bus in a DP600?

I appreciate

Thanks

Antonio