PLUS+1 Hardware > Displays
Display Buzzer
(1/1)
Mike AA:
I am looking at the outputs on the DM1200 and data sheet and I don't see if the buzzer is simply an output port or if there is an actual buzzer built into the display. Under buzzer it doesn't give me a port to connect to. I the data sheet there is no discussion of where to connect externally.
Help please?
Mike
A.Fitz:
Hey Mike,
Looking at the guide template, looks like the buzzer is built into the display, see attached image.
Mike AA:
A.Fitz,
That is exactly what I see and when I enable the buzzer with the default volume and frequency I don't hear anything.
I have my service tool monitoring the signal and it shows I am enabling it.
Mike
Tor:
Hi,
No, there is no built in buzzer in the DM1x00. The name on the output is a bit misleading.
Here's a video that explains how to get the "buzzer" and sound going: https://www.youtube.com/watch?v=Qip8rPAA8mI
I hope it helps.
Have a nice day.
Navigation
[0] Message Index
Go to full version