Author Topic: Use PEAK-to-USB for Plus+1 service tool  (Read 5304 times)

Offline Morten Rosengreen

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Use PEAK-to-USB for Plus+1 service tool
« on: June 03, 2022, 12:17:09 PM »
Hello Forum

I have bought a couple of PEAK-gateways, but noticed that they are not compatible with Danfoss Plus+1 directly.

Then I found out that it should be possible to make it work.

Can anyone tell me how to implement the PEAK-gateway in the servicetool?

BR Morten

Offline tronelec

  • PLUS+1 Developer
  • ***
  • Posts: 19
  • Karma: +0/-1
Re: Use PEAK-to-USB for Plus+1 service tool
« Reply #1 on: July 26, 2022, 09:47:51 PM »
hola, estoy en tu misma situación, aunque los manuales de servicetool indica que las interfaz deben cumplir con protocolo rp1210a/b, al instalar la interfaz peak esta no aparece como intefaz disponible para seleccionar desde servicetool, estoy viendo una configuracion adicional de la interfaz desde panel de control de windows, adicionalmente usted puede  ver un archivo que se agrego a rp1210 desde servicetool, dentro de servicetool presionar ctrl+alt+l

esto aparece:

--PEAKRP32
   Parsing: PEAKRP32
   Parse results for: C:\WINDOWS\PEAKRP32.ini:
      Name:        PEAK-System PCAN Adapter
      Address1:    Otto-Roehm str. 69
      Address2:    (Not specified)
      City:        Darmstadt
      Country:     Germany
      State:       Hessen
      Postal:      64293
      Telephone:   0049-6151-817320
      Fax:         0049-6151-817329
      VendorURL:   http://www.peak-system.com
      Version:     3.0
      RP1210 Version:    C
      *** WARNING *** [C:\WINDOWS\PEAKRP32.ini]   Gateway uses C. PLUS+1 Service Tool is tested with RP1210A and RP1210B.

      CANFormatsSupported:    3,4,5
      Protocols:       10,20,30
      Devices:       

      C:\WINDOWS\system32\PEAKRP32.dll exported functions:
         ClearRegisteredDevices
         GetLicenseInfo
         GetLicenseStatus
         RP1210_ClientConnect
         RP1210_ClientDisconnect
         RP1210_GetErrorMsg
         RP1210_GetHardwareStatus
         RP1210_GetLastErrorMsg
         RP1210_Ioctl
         RP1210_ReadDetailedVersion
         RP1210_ReadMessage
         RP1210_ReadVersion
         RP1210_SendCommand
         RP1210_SendMessage
         RegisterAttachedDevices
         RegisterPEAKRP1210
         RegisterRPDevice
         UnregisterPEAKRP1210
         UnregisterRPDevice


al parecer se instalo como PROTOCOLA RP1210 C  :o
      --
« Last Edit: July 26, 2022, 10:50:52 PM by tronelec »

Offline tronelec

  • PLUS+1 Developer
  • ***
  • Posts: 19
  • Karma: +0/-1
Re: Use PEAK-to-USB for Plus+1 service tool
« Reply #2 on: July 26, 2022, 11:18:28 PM »
desde https://www.peak-system.com/Software-Information.77.0.html?&L=1&no_cache=1&sword_list%5B0%5D=pcanrp1210a  , no esta disponible el paquete de instalación para PCAN-RP1210-A API, se debe contactar con el fabricante.

acá indica que el desarrollo de rp1210A Esta descontinuado por peak system , aunque indica que es gratuito no veo el link de descarga
https://www.peak-system.com/PCAN-RP1210-A.143.0.html?&L=1

si lo consigo lo compartiré

Offline tronelec

  • PLUS+1 Developer
  • ***
  • Posts: 19
  • Karma: +0/-1
Re: Use PEAK-to-USB for Plus+1 service tool
« Reply #3 on: July 28, 2022, 03:34:28 AM »
adjunto rp1210 A, para peak system

Offline tronelec

  • PLUS+1 Developer
  • ***
  • Posts: 19
  • Karma: +0/-1
Re: Use PEAK-to-USB for Plus+1 service tool
« Reply #4 on: July 28, 2022, 03:42:03 AM »
aca print de pantalla, select gateway modo virtual


Offline Morten Rosengreen

  • PLUS+1 Novice
  • *
  • Posts: 2
  • Karma: +0/-0
Re: Use PEAK-to-USB for Plus+1 service tool
« Reply #5 on: August 03, 2022, 09:28:33 AM »
Thanks for reply
Did you manage to find the correct file?

I have tried, but could see the log for the RP1210:
Parse results for: C:\WINDOWS\RP121032.INI:

--PEAKRP32
   Parsing: PEAKRP32
   Parse results for: C:\WINDOWS\PEAKRP32.ini:
      Name:        PEAK-System PCAN Adapter
      Address1:    Otto-Roehm str. 69
      Address2:    (Not specified)
      City:        Darmstadt
      Country:     Germany
      State:       Hessen
      Postal:      64293
      Telephone:   0049-6151-817320
      Fax:         0049-6151-817329
      VendorURL:   http://www.peak-system.com
      Version:     3.0
      RP1210 Version:    C
      *** WARNING *** [C:\WINDOWS\PEAKRP32.ini]   Gateway uses C. PLUS+1 Service Tool is tested with RP1210A and RP1210B.

      CANFormatsSupported:    3,4,5
      Protocols:       10,20,30
      Devices:       

      C:\WINDOWS\system32\PEAKRP32.dll exported functions:
         ClearRegisteredDevices
         GetLicenseInfo
         GetLicenseStatus
         RP1210_ClientConnect
         RP1210_ClientDisconnect
         RP1210_GetErrorMsg
         RP1210_GetHardwareStatus
         RP1210_GetLastErrorMsg
         RP1210_Ioctl
         RP1210_ReadDetailedVersion
         RP1210_ReadMessage
         RP1210_ReadVersion
         RP1210_SendCommand
         RP1210_SendMessage
         RegisterAttachedDevices
         RegisterPEAKRP1210
         RegisterRPDevice
         UnregisterPEAKRP1210
         UnregisterRPDevice
      --
      Attempting to add protocol: 10
      Protocol: 10
         ProtocolDescription:    CAN Network Protocol
         ProtocolString:    CAN
         ProtocolSpeed:       125,250,500,1000,Auto
         ProtocolParams:    
         Devices:       
      *** SKIPPED *** This protocol has no useable devices!

      Failed to add protocol: 10
      --
      Attempting to add protocol: 20
      Protocol: 20
         ProtocolDescription:    SAE J1939 Protocol
         ProtocolString:    J1939
         *** SKIPPED *** "ProtocolString" must be CAN

      Failed to add protocol: 20
      --
      Attempting to add protocol: 30
      Protocol: 30
         ProtocolDescription:    ISO15765 Vehicle Protocol
         ProtocolString:    ISO15765
         *** SKIPPED *** "ProtocolString" must be CAN

      Failed to add protocol: 30
      *** WARNING *** [C:\WINDOWS\PEAKRP32.ini]   Generic CAN protocol is not supported.

      --
      Attempting to add protocol: 10
      Protocol: 10
         ProtocolDescription:    CAN Network Protocol
         ProtocolString:    CAN
         *** SKIPPED *** "ProtocolString" must be J1939

      Failed to add protocol: 10
      --
      Attempting to add protocol: 20
      Protocol: 20
         ProtocolDescription:    SAE J1939 Protocol
         ProtocolString:    J1939
         ProtocolSpeed:       125,250,500,1000,Auto
         ProtocolParams:    
         Devices:       
      *** SKIPPED *** This protocol has no useable devices!

      Failed to add protocol: 20
      --
      Attempting to add protocol: 30
      Protocol: 30
         ProtocolDescription:    ISO15765 Vehicle Protocol
         ProtocolString:    ISO15765
         *** SKIPPED *** "ProtocolString" must be J1939

      Failed to add protocol: 30
         *** ERROR *** [C:\WINDOWS\PEAKRP32.ini]   No valid protocols (The Generic CAN or J1939 protocol is needed by PLUS+1 Service Tool)

   Failed to parse: C:\WINDOWS\PEAKRP32.ini
*** WARNING *** No RP1210 vendor files parsed successfully