Author Topic: Pulse which holds sinal for duration even if input signal goes T/F.  (Read 6842 times)

ET

  • Guest
The help docs state that the Pulse component will output false if the input goes T/F during the hold time.
Is there another component which will continue to output true for the entire hold time, even if the input goes T/F during the hold time?
If not, is there an easy way to wire this function up using other components?

Offline A.Peterson

  • PLUS+1 User
  • **
  • Posts: 7
  • Karma: +0/-0
Re: Pulse which holds sinal for duration even if input signal goes T/F.
« Reply #1 on: April 16, 2012, 07:25:48 PM »
Use a positive transition into a delay off and you can set the length of pulse to whatever you want regardlees of the input state.

ET

  • Guest
Re: Pulse which holds sinal for duration even if input signal goes T/F.
« Reply #2 on: April 17, 2012, 07:09:17 PM »
Ah, that sounds like it will work nicely.
Thanks!