PLUS+1 Software > Function Library
Problem with Widget library
(1/1)
samuelhj:
Hello.
Been a while since I had to program a display, but I'm running into two seperate issues.
Display type: DM430E 0-1-X-X series.
Guide version 2024.4.3
If I add a gauge, adjust parameters, and try to compile I get compiler error.
See attached screenshots.
Another strange issue I noticed, linear gauges do not even fit the display, but since I've never used them, I'm not sure if this is expected behaviour?
Navigation
[0] Message Index
Go to full version