PLUS+1 Hardware > Controllers
SC050_C1P46_Status_128_Problem
(1/1)
macbahi:
Hi,
Any controller I use (Sc024 or SC050) to set ON coil using digital output as C1P46 to controller give me error C1P46 status=128 as showing in picture.
I must to reset the controller even though the output was set off. And the current was correct around 1,4A.
The error occurring after a few minutes that everything was working fine. Sometimes the error appears in a little time and sometimes more time.
Coil is sun 770-214 14V 8.9Ohm and DIN connector S18209TC411.
Please where is the problem?
Thank you very much
With best regards
Navigation
[0] Message Index
Go to full version